Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2015-06-08 2.41 L4411A Firmware Update Revision 2.41.
Release Date Version
2015-06-08 2.41
Version Description
L4411A Firmware Update Revision 2.41.

How to Download

  1. Download and install the L4411A Firmware Update Utility located in the "Add-On Software/Utilities" section at the bottom of this page. If you already have the Firmware Update Utility installed on your computer, skip this step.
  2. Use the Download button to download the Keysight L4411A Firmware.
  3. Unzip the Keysight L4411A Firmware file, making note of where you store the unzipped file.
  4. Open the Firmware Update Utility (Start -> Programs -> Keysight -> Firmware Update Utility).
  5. Click Next.

How to Install

  1. Click Browse and locate the firmware update file that you unzipped. Highlight the file and select Open.
  2. Click Next.
  3. Select the I/O interface (GPIB, LAN, or USB) that connects your DMM to your PC.
  4. Choose the settings necessary for communication (GPIB address, IP address, USB ID).
  5. Click Update. NOTE: This update will take several minutes and the DMM will display status messages and automatically reboot when completed. DO NOT cycle or interrupt power to the DMM during the update process.
  6. After this is completed, exit the update utility.
  7. Refer to the DMM front panel and note if there are any errors (the ERROR light will be on in the display).
  8. The update process is now complete.

Note: There is no need to re-calibrate the DMM when this new firmware is installed.
 

Licensing

  • Does Not Require a License

Installs on: Instrument

Prerequisites

  • No specific prerequisites.

Supported Instruments

  • L4411A
No previous versions available
SHOW MORE