IO Libraries Suite Downloads
To find out more about the IO Libraries Suite, visit www.keysight.com/find/iosuite
IO Libraries Suite 2020 Update 1 offers two significant changes from the previous software version:
- It fixes the discovery process for the 1394-VXI interface when the VXI system is using MXI connections.
- It fixes the memory leaking issues in the Keysight Instrument Discovery Service and LxiMdnsBrowser.
The remaining enhancements in this list were made for IO Libraries Suite 2020.
- General performance enhancements.
- VISA Shared Components - Upgrade to 5.12.
- Support for GPIB drivers with Windows 10 Device Guard.
-
Bug fixes and minor enhancements including:
- When NI is the primary resource manager, Connection Expert now reports all NI PXI modules.
- On systems with NI VISA, an install repair operation completes fully.
- When the NI PXI system module is used with Keysight Resource Manager as the primary resource manager, the full address of the system module is now reported correctly.
- Serial instrument detection is fixed.
- Following an upgrade, the GPIB instrument list is properly refreshed.
- Checking status on a LAN instrument completes without interrupting instrument discovery.
- Serial ports, which were not displaying in Connection Expert in certain configurations, are now visible.
- Following an upgrade, the GPIB instrument list is properly refreshed.
- Checking status on a LAN instrument completes without interrupting instrument discovery.
- Serial ports, which were not displaying in Connection Expert in certain configurations, are now visible.
Release Date | Version | Version Description |
---|---|---|
2020-10-15 | 2020 Update 1 | See description above. Build 18.1.26209.5 |
How to Download
- Click the download link and save the installer.
How to Install
- Run the downloaded installer with Admin Privilege.
Licensing
- Does Not Require a License
Supporting Documentation
Download
Installs on:
PC
Operating System
- Windows 10 v1809 and above
- Windows 8.1 Enterprise
- Windows 7 SP1 Enterprise
Prerequisites
- For Windows 10: .NET Framework 3.5/2.0 installed