検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

53230A Firmware

Update to reduce the occurrence of a memory leak.

リリース バージョン 内容
2019-10-07 3.02 Firmware update 3.02

ダウンロード方法

  1. Click the Download button.
  2. Save the firmware file to your computer and note the directory where the file is saved. Firmware updates installed over the LAN, GPIB, or USB interface are files with .upd extensions.
  3. Unzip the file to access the .upd file. For updates using a front panel USB drive, the utility extracts the required files from the (unzipped) .upd file.
  4. If not currently installed, download and install the Firmware Update Utility.

インストール方法

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation.
  • If updating from the LAN, USB, or GPIB interface the instrument address is required. With the instrument turned on, pressing Help ­ About displays the addresses.
    The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
  • It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.­

ライセンス

  • ライセンス不要

説明資料

アドオン・ソフトウェア/ユーティリティ

ダウンロード

インストール:

Instrument

OS

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP
  • Windows 10

前提条件

  • ドキュメントはありません

対象測定器

  • 53230A