Situation:

After April 18th 2018, i1000 software will report a “VTEP License Not found” error during start-up, VTEP learning or VTEP diagnostics, even though the license file is valid.

The i1000 software, including the VTEP software will continue to function in production, however VTEP learning, debugging and diagnostics functionalities will not work any more.

This issue happens across all i1000D system types and all versions of the software.

Solution/Action:

A software issue has been identified and a software patch has been created and is available for download.

After downloading, the “VTEP_Fix_setup.exe” can be run directly and after restarting i1000 software, the error message will not show up and VTEP should be working as it is desired.
 

是德建议使用最新的版本,其中包括最新的漏洞修复和安全补丁
发布日期 版本 版本说明
2018-04-27 NA Hot fix to resolve VTEP error
发布日期 版本
2018-04-27 NA
Version Description
Hot fix to resolve VTEP error

如何下载

  • Click the "Download" button.
    Save file to a folder in C: drive of PC.

如何安装

  • Double click on the downloaded file.

颁发许可证

  • Does Not Require a License

Installs on: PC

操作系统

  • Windows 7

前提要求

  • No prerequisite required.

没有可用的软件版本
SHOW MORE