Here’s the page we think you wanted. See search results instead:

 

Contactar a un Experto

New Bootpt.exe file for i3070

You can install a newer version of BOOTP Turbo software to resolve the boot issue.

Installation Procedure:

1. Download the “bootpt.exe”.
2. Back up the bootptab file in c:\Windows\system32\drivers\etc by renaming it to bootptab.org.
3. Go to Control Panel > Programs and Features, Remove BOOTP Turbo software
4. To install the newer version, double click on “bootpt.exe”
5. Follow the instruction to complete the installation.
6. Rename bootptab.org to bootptab in c:\Windows\system32\drivers\etc.
7. Restart the PC.

*Microsoft and Windows are trademarks or registered trademarks of Microsoft Corporation in the United States and/or other countries.

Situation:
The i3070 Series 5 test system controller that installed i3070 software 09.10p with Windows 7 Operating System may encounter testhead boot-up issue as shown below.

The Bootp Turbo software used in 9.10p is having some conflicts with certain types of PC controller. This could happen to newly shipped systems, or existing systems upgraded from earlier software revision.

 

Validation:
Locate bootpt.exe at “C:\Program Files (x86)\BOOTP Turbo\bootpt.exe”, right click mouse and select the “Properties”, then select “Details” tab as shown below:

The correct Product version is “1.3.0.1252” and the Copyright is “Copyright@1996-2012

 

Solution/Action:
Install a newer version of BOOTP Turbo software could resolved the issue.
 

Please refer to Service Note 3070-89a for details

Publicación Versión Descripción
2018-05-10 NA Bootp to resolve testhead boot error in software version 09.10p

¿Cómo descargarlo?

  • Información No Disponible

¿Cómo instalarlo?

  • Información No Disponible

Licencias

  • No Requiere Licencia
Descargar

Instalación en::

PC

Sistema Operativo

  • Windows 7

Pre-requisitos

  • Información No Disponible

Instrumentos Soportados

  • i3070