*********************** **** Read Me First **** *********************** Version: 1.1.1 Jul 2018 Introducing the Keysight LabVIEW Driver for Keysight XSAnRadioTest --------------------------------------------------------------------------- This instrument driver provides access to RadioTest measurement application for AgXSAn host driver through LabVIEW VIs. Supported Models --------------------- M8920A Requirement ----------- LabVIEW 8.5 or later Installation ------------- System Requirements: The driver installation will check for the following requirements. If not found, the installer will either abort, warn, or install the required component as appropriate. Supported Operating Systems: Windows 7 32-bit, 64-bit Windows 8 32-bit, 64-bit Windows 10 32-bit, 64-bit IVI Driver: Before this driver can be installed, your computer must already have: Driver Name: Base - X-Series Signal Analyzers IVI Driver (AgXSAn IVI Driver version 3.5.6.0 or greater) Driver Name: Radio Test - X-Series Signal Analyzers IVI Driver (KtXSAnRadioTest IVI Driver version 1.0.7.0 or greater). The IVI Driver installers are available from: http://www.keysight.com/find/sa-ivi Dependency ---------- This LabVIEW driver has a dependency on Keysight XSAn LabVIEW driver version 1.0.3 or greater. So prior to the installation of this driver, please install the XSAn LabVIEW driver from following link. To download, please visit: http://www.keysight.com/find/sa-ivi Uninstall --------- This driver can be uninstalled like any other software from the Control Panel using "Programs and Features" in Windows 7/Windows 8/Windows 8.1/Windows 10. LabVIEW driver VIs, Help File and example VIs --------------------------------------------- All the driver VIs are added in the "instr.lib" under the LabVIEW directory. A help file is added in the LabVIEW help directory. It contains a brief description of all the VIs belongs to the LabVIEW driver. Some example VIs are also added in the example directory for the LabVIEW driver. IVI Instrument Class supported ------------------------------ IVI Instrument Class: None Revision History ---------------- Revision History ---------------- Version 1.1.1 Date Jul 2018 Notes Initial public release. More Information ---------------- For more information about this driver and other instrument drivers and software available from Keysight Technologies visit: http://www.keysight.com/find/drivers A list of contact information is available from: http://www.keysight.com/find/contactus Copyright Keysight Technologies 2018