*********************** **** Read Me First **** *********************** Version 1.0.0 Aug 2020 Introducing the Keysight LabVIEW Driver for KtDAQ970. --------------------------------------------------------------------------- This instrument driver provides access to the functionality of KtDAQ970A through LabVIEW VIs. Supported Models --------------------- 34970A, 34972A, DAQ970A, DAQ973A Requirement ----------- LabVIEW 8.5 or Later Installation ------------- System Requirements: The driver installation will check for the following requirements. If not found, the installer will either abort, warn, or install the required component as appropriate. Supported Operating Systems: Windows 7 32-bit, 64-bit Windows 8 32-bit, 64-bit Windows 10 32-bit, 64-bit IVI Drivers: Before this driver can be installed, your computer must already have: Driver Name: DAQ970 Data Acquisition System IVI Driver (KtDAQ970 IVI-C Driver for the Keysight Data Acquisition System version 1.0.0.0 or greater) The IVI Driver installers are available from: https://www.keysight.com/main/software.jspx?ckey=2991469&lc=eng&cc=US&nid=-11143.0.00&id=2991469 Uninstall --------- This driver can be uninstalled like any other software from the Control Panel using "Programs and Features" in Windows 7/Windows 8/Windows 10. LabVIEW driver VIs, Help File and example VIs --------------------------------------------- All the driver VIs are added in the "instr.lib" under the LabVIEW directory. A help file is added in the LabVIEW help directory. It contains a brief decription of all the VIs belongs to the LabVIEW driver. Some example VIs are also added in the example directory for the LabVIEW driver. IVI Instrument Class supported ------------------------------ IVI Instrument Class: None Revision History ---------------- Version Date Notes ------- --------- ----------------------- 1.0.0 Aug 2020 Initial public release(based on IVI-C version 1.0.0.0) More Information ---------------- For more information about this driver and other instrument drivers and software available from Keysight Technologies visit: http://www.keysight.com/find/drivers A list of contact information is available from: http://www.keysight.com/find/contactus Copyright Keysight Technologies 2020