*********************** **** Read Me First **** *********************** Version: 1.3.2 August 2018 Introducing the Keysight LabVIEW Driver for the Keysight XSAnBasic --------------------------------------------------------------------------- This instrument driver provides access to the functionality of the IQ Analyzer through LabVIEW VIs. Supported Instruments --------------------- N9020A, N9020B, N9010A, N9010B, N9030A, N9030B, N9000A, N9000B, M9290A, N9040B, N9041B, N9038A, M9420A, M9421A, SPN9003A, SPN9026A, N8973B, N8974B, N8975B, N8976B, M90XA, M8920A Requirement ----------- LabVIEW 8.5 or later Installation ------------- System Requirements: The driver installation will check for the following requirements. If not found, the installer will either abort, warn, or install the required component as appropriate. Supported Operating Systems: Windows 7 32-bit, 64-bit Windows 8 32-bit, 64-bit Windows 10 32-bit, 64-bit IVI Drivers: Before this driver can be installed, your computer must already have: Driver Name: Base - X-Series Signal Analyzers IVI Driver (AgXSAn IVI Driver version 3.5.6.0 or greater) and Driver Name: I/Q Analyzer Basic - X-Series Signal Analyzers IVI Driver (AgXSAnBasic IVI Driver version 1.3.3.0 or greater). The IVI Driver installers are available from: http://www.keysight.com/find/sa-ivi Dependency ---------- This LabVIEW driver has a dependency on Keysight XSAn LabVIEW driver version 1.0.3 or greater. So prior to the installation of this driver, please install the XSAn LabVIEW driver from following link. To download, please visit: http://www.keysight.com/find/sa-ivi Uninstall --------- This driver can be uninstalled like any other software from the Control Panel using "Programs and Features" in Windows 7/Windows 8/Windows 8.1/Windows 10. LabVIEW driver VIs, Help File and example VIs --------------------------------------------- All the driver VIs are added in the "instr.lib" under the LabVIEW directory. A help file is added in the LabVIEW help directory. It contains a brief description of all the VIs belongs to the LabVIEW driver. Some example VIs are also added in the example directory for the LabVIEW driver. IVI Instrument Class supported ------------------------------ None Known Issues ------------ None Note: To report issues or provide feedback about this instrument driver, please send an email to ividrivers_support@keysight.com. Revision History ---------------- Version 1.3.2 Date Aug 2018 Notes Resolved Defects Version 1.1.0 Date Dec 2017 Notes Updated driver to support 'B' model of instruments. Version 1.0.0 Date Dec 2015 Notes Initial public release. More Information ---------------- For more information about this driver and other instrument drivers and software available from Keysight Technologies visit: http://www.keysight.com/find/drivers A list of contact information is available from: http://www.keysight.com/find/contactus Copyright Keysight Technologies 2015-2018