=============================================== README.TXT EasyEXPERT group+ (for B150x mainframe) =============================================== This document contains the following: * Note * Software Requirements * Update Instructions Note ==== Remote Control Interface is not supported on B1500A that runs on Windows XP. Software Requirements ===================== In order to update the EasyEXPERT Rev. A.05.04 or prior revisions to Rev. A.05.50 or later revisions, the following software is required. - Microsoft Windows Installer 3.1 - Microsoft .NET Framework 3.5 Service Pack 1 NOTE: If all the required software has not been installed to your computer, install them in the above sequence. For example, if Microsoft Windows Installer 3.1 is not installed, install it, and then install Microsoft .NET Framework 3.5 Service Pack 1. The required software is stored in the "Prerequisites" folder in this Package. Update Instructions =================== To update the EasyEXPERT for B1500, follow the procedure below. 1. If the downloaded file is saved to a PC, copy it to B150xA by using a media such as CD-R/DVD-R/USB memory. 2. On B150xA, if you see [Start EasyEXPERT] button on the screen, close the window by clicking "x" button on the window title bar. 3. Expand the contents of the downloaded file into a working folder as follows. a) Go to the folder where the downloaded file is saved and open the folder. b) Place the pointer on the downloaded file and click the mouse right bitton and select "Extract All...". NOTE: If any unzip tool is installed, the above may not work. In this case, follow the instruction of the tool. Below is an example for the tool "winzip". - Firstly double-click the downloaded file, then click "unzip" in the menu bar. Then specify the folder and click "unzip". 4. Double click the EasyEXPERT folder. 5. Click the executable file to start the installation and follow the instructions of the setup wizard. 6. Wait for installation to complete, and restart the B150xA. Microsoft and Windows are registered trademarks of Microsoft Corporation. All other trademarks are the property of their respective owners. Copyright Keysight Technologies 2006 - 2018 All rights reserved.