MXG Signal Generator Upgrade Assistant FAQ's
These FAQ's contain troubleshooting information about Keysight Technologies MXG signal generator upgrade assistant.
I am new to the MXG upgrade assistant, wheredo I get help?
The upgrade was interrupted, what do I do now?
During the upgrade I see a few errors onthe instrument. Are they expected?
Is it advisable to upgrade a signal generator with multiple signal generators turned on?
How do I configure the PC's LAN settings to upgrade using a cross-over LAN cable?
Why can't I choose USB as the upgrade connection type?
Why can't I use a USB alias when choosing the upgrade connection type?
Why does the USB upgrade time out after rebooting the instrument?
Learn more about X-Series Signal Generators (MXG, EXG, CXG)