Starting Download..
save Save

How do I upgrade my ENA Series Network Analyzer?

Following upgrades are available for the E5070B, E5071B and E5071C. The upgrades in most cases are Firmware updates, Hardware upgrades and Software upgrades.
The upgrades contents are described in the table below.

Windows Upgrade Kit Information

For E5071C user, it is prepared the following upgrades:

2-1-1. Frequency upgrade
2-1-2. Lower frequency limit upgrade
2-1-3. Port up
2-1-4. Add bias tees

These upgrades are prepared for the E5071C only, and be sure that the upgrade options listed in the following "Upgrade path for frequency, port up, and add bias tees" need to be ordered (e.g. To upgrade the unit from Opt. 240 to Opt. 480, order "E5071CU-300" and "E5071CU-480" respectively).

"Add high stability timebase" and "Upgrade to removable HDD" can be ordered independently with the upgrade options for frequency upgrade, lower frequency limit upgrade, port, up, and add bias tees.

The parts in our upgrade kits come with a 90-day warranty against any manufacturing defect. The warranty period of the instrument into which they are installed is not affected.

1. Firmware Updates

The firmware updates can be downloaded from the url below. The following url also contains the installation, and firmware update history.

2. Hardware Upgrades

Upgrade path for frequency, port up, and bias tees
ModelOption (From) Option (To)Upgrade Kit combination (Windows XP)Upgrade Kit combination (Windows 7)
Upgrade Kit combination (Windows 10)1






E5071C


  

       





        240


      

      245  E5071CU-100 E5071CU-100E5071CU-100
      260 E5071CU-260  E5071CU-260E5071CU-260
      265 E5071CU-100 + E5071CU-265 E5071CU-100 + E5071CU-265E5071CU-100 + E5071CU-265
      280 E5071CU-280 E5071CU-280E5071CU-280
      285 E5071CU-100 + E5071CU-285 E5071CU-100 + E5071CU-285E5071CU-100 + E5071CU-285
      440 E5071CU-300 E5071CU-370E5071CU-390
      445 E5071CU-100 + E5071CU-301 E5071CU-100 + E5071CU-371E5071CU-100 + E5071CU-391
      460 E5071CU-260 + E5071CU-305 E5071CU-260 + E5071CU-375E5071CU-260 + E5071CU-395
      465 E5071CU-100 + E5071CU-265 + E5071CU-306 E5071CU-100 + E5071CU-265 + E5071CU-376E5071CU-100 + E5071CU-265 + E5071CU-396
      480 E5071CU-280 + E5071CU-302 E5071CU-280 + E5071CU-372E5071CU-280 + E5071CU-392
      485 E5071CU-100 + E5071CU-285+ E5071CU-303 E5071CU-100 + E5071CU-285+ E5071CU-373E5071CU-100 + E5071CU-285+ E5071CU-393
      2D5 E5071CU-280 + E5071CU-2D5 E5071CU-280 + E5071CU-2D7E5071CU-280 + E5071CU-2D8
      4D5 E5071CU-280 + E5071CU-2D5 + E5071CU-307 E5071CU-280 + E5071CU-2D7 + E5071CU-377E5071CU-280 + E5071CU-2D8 + E5071CU-397
      2K5 E5071CU-280 + E5071CU-2K5 E5071CU-280 + E5071CU-2K7E5071CU-280 + E5071CU-2K8
      4K5 E5071CU-280 + E5071CU-2K5 + E5071CU-304 E5071CU-280 + E5071CU-2K7 + E5071CU-374E5071CU-280 + E5071CU-2K8 + E5071CU-394






E5071C 


 







        245

     

    

      240E5071CU-200 E5071CU-200E5071CU-200
      260  E5071CU-200 + E5071CU-260 E5071CU-200 + E5071CU-260E5071CU-200 + E5071CU-260
      265 E5071CU-265 E5071CU-265E5071CU-265
      280 E5071CU-200 + E5071CU-280 E5071CU-200 + E5071CU-280E5071CU-200 + E5071CU-280
      285 E5071CU-285 E5071CU-285E5071CU-285
      440 E5071CU-200 + E5071CU-300 E5071CU-200 + E5071CU-370E5071CU-200 + E5071CU-390
      445 E5071CU-301 E5071CU-371E5071CU-391
      460 E5071CU-200 + E5071CU-260 + E5071CU-305 E5071CU-200 + E5071CU-260 + E5071CU-375E5071CU-200 + E5071CU-260 + E5071CU-395
      465 E5071CU-265 + E5071CU-306 E5071CU-265 + E5071CU-376E5071CU-265 + E5071CU-396
      480 E5071CU-200 + E5071CU-280 + E5071CU-302 E5071CU-200 + E5071CU-280 + E5071CU-372E5071CU-200 + E5071CU-280 + E5071CU-392
      485 E5071CU-285 + E5071CU-303 E5071CU-285 + E5071CU-373E5071CU-285 + E5071CU-393
      2D5 E5071CU-285 + E5071CU-2D5 E5071CU-285 + E5071CU-2D7E5071CU-285 + E5071CU-2D8
      4D5 E5071CU-285 + E5071CU-2D5 + E5071CU-307 E5071CU-285 + E5071CU-2D7 + E5071CU-377E5071CU-285 + E5071CU-2D8 + E5071CU-397
      2K5 E5071CU-285 + E5071CU-2K5 E5071CU-285 + E5071CU-2K7E5071CU-285 + E5071CU-2K8
      4K5 E5071CU-285 + E5071CU-2K5 + E5071CU-304 E5071CU-285 + E5071CU-2K7 + E5071CU-374E5071CU-285 + E5071CU-2K8 + E5071CU-394





E5071C





        260

      265 E5071CU-104 E5071CU-104E5071CU-104
      280 E5071CU-281 E5071CU-281E5071CU-281
      285 E5071CU-104 + E5071CU-286 E5071CU-104 + E5071CU-286E5071CU-104 + E5071CU-286
      460 E5071CU-305 E5071CU-375E5071CU-395
      465 E5071CU-104 + E5071CU-306 E5071CU-104 + E5071CU-376E5071CU-104 + E5071CU-396
      480 E5071CU-281 + E5071CU-302 E5071CU-281 + E5071CU-372E5071CU-281 + E5071CU-392
      485 E5071CU-104 + E5071CU-286 + E5071CU-303 E5071CU-104 + E5071CU-286 + E5071CU-373E5071CU-104 + E5071CU-286 + E5071CU-393
      2D5 E5071CU-281 + E5071CU-2D5 E5071CU-281 + E5071CU-2D7E5071CU-281 + E5071CU-2D8
      4D5 E5071CU-281 + E5071CU-2D5 + E5071CU-307 E5071CU-281 + E5071CU-2D7 + E5071CU-377E5071CU-281 + E5071CU-2D8 + E5071CU-397
      2K5 E5071CU-281 + E5071CU-2K5 E5071CU-281 + E5071CU-2K7E5071CU-281 + E5071CU-2K8
      4K5 E5071CU-281 + E5071CU-2K5 + E5071CU-304 E5071CU-281 + E5071CU-2K7 + E5071CU-374E5071CU-281 + E5071CU-2K8 + E5071CU-394





E5071C





        265

      260 E5071CU-204 E5071CU-204E5071CU-204
      280 E5071CU-204 + E5071CU-281 E5071CU-204 + E5071CU-281E5071CU-204 + E5071CU-281
      285 E5071CU-286 E5071CU-286E5071CU-286
      460 E5071CU-204 + E5071CU-305 E5071CU-204 + E5071CU-375E5071CU-204 + E5071CU-395
      465 E5071CU-306 E5071CU-376E5071CU-396
      480 E5071CU-204 + E5071CU-281 + E5071CU-302 E5071CU-204 + E5071CU-281 + E5071CU-372E5071CU-204 + E5071CU-281 + E5071CU-392
      485 E5071CU-286 + E5071CU-303 E5071CU-286 + E5071CU-373E5071CU-286 + E5071CU-393
      2D5 E5071CU-286 + E5071CU-2D5 E5071CU-286 + E5071CU-2D7E5071CU-286 + E5071CU-2D8
      4D5 E5071CU-286 + E5071CU-2D5 + E5071CU-307 E5071CU-286 + E5071CU-2D7 + E5071CU-377E5071CU-286 + E5071CU-2D8 + E5071CU-397
      2K5 E5071CU-286 + E5071CU-2K5 E5071CU-286 + E5071CU-2K7E5071CU-286 + E5071CU-2K8
      4K5 E5071CU-286 + E5071CU-2K5 + E5071CU-304 E5071CU-286 + E5071CU-2K7 + E5071CU-374E5071CU-286 + E5071CU-2K8 + E5071CU-394




E5071C



       

        280

      285 E5071CU-101 E5071CU-101E5071CU-101
      480 E5071CU-302 E5071CU-372E5071CU-392
      485 E5071CU-101 + E5071CU-303 E5071CU-101 + E5071CU-373E5071CU-101 + E5071CU-393
      2D5 E5071CU-2D5 E5071CU-2D7E5071CU-2D8
      4D5 E5071CU-2D5 + E5071CU-307 E5071CU-2D7 + E5071CU-377E5071CU-2D8 + E5071CU-397
      2K5 E5071CU-2K5 E5071CU-2K7E5071CU-2K8
      4K5 E5071CU-2K5 + E5071CU-304 E5071CU-2K7 + E5071CU-374E5071CU-2K8 + E5071CU-394



E5071C



        285

      280 E5071CU-201 E5071CU-201E5071CU-201
      480 E5071CU-201 + E5071CU-302 E5071CU-201 + E5071CU-372E5071CU-201 + E5071CU-392
      485 E5071CU-303 E5071CU-373E5071CU-393
      2D5 E5071CU-2D5 E5071CU-2D7E5071CU-2D8
      4D5 E5071CU-2D5 + E5071CU-307 E5071CU-2D7 + E5071CU-377E5071CU-2D8 + E5071CU-397
      2K5 E5071CU-2K5 E5071CU-2K7E5071CU-2K8
      4K5 E5071CU-2K5 + E5071CU-304 E5071CU-2K7 + E5071CU-374E5071CU-2K8 + E5071CU-394


E5071C


        2D5

      2K5 E5071CU-2K6 E5071CU-2K6E5071CU-2K6
      4D5 E5071CU-307 E5071CU-377E5071CU-397
      4K5 E5071CU-2K6 + E5071CU-304 E5071CU-2K6 + E5071CU-374E5071CU-2K6 + E5071CU-394
E5071C        2K5      4K5 E5071CU-304 E5071CU-374E5071CU-394



E5071C



        440

      445 E5071CU-102 E5071CU-102E5071CU-102
      460 E5071CU-460 E5071CU-460E5071CU-460
      465 E5071CU-102 + E5071CU-465 E5071CU-102 + E5071CU-465E5071CU-102 + E5071CU-465
      480 E5071CU-480 E5071CU-480E5071CU-480
      485 E5071CU-102 + E5071CU-485 E5071CU-102 + E5071CU-485E5071CU-102 + E5071CU-485
      4D5 E5071CU-480 + E5071CU-4D5 E5071CU-480 + E5071CU-4D7E5071CU-480 + E5071CU-4D8
      4K5 E5071CU-480 + E5071CU-4K5 E5071CU-480 + E5071CU-4K7E5071CU-480 + E5071CU-4K8




E5071C




        445

      440 E5071CU-202 E5071CU-202E5071CU-202
      460 E5071CU-202 + E5071CU-460 E5071CU-202 + E5071CU-460E5071CU-202 + E5071CU-460
      465 E5071CU-465 E5071CU-465E5071CU-465
      480 E5071CU-202 + E5071CU-480 E5071CU-202 + E5071CU-480E5071CU-202 + E5071CU-480
      485 E5071CU-485 E5071CU-485E5071CU-485
      4D5 E5071CU-485 + E5071CU-4D5 E5071CU-485 + E5071CU-4D7E5071CU-485 + E5071CU-4D8
      4K5 E5071CU-485 + E5071CU-4K5 E5071CU-485 + E5071CU-4K7E5071CU-485 + E5071CU-4K8



E5071C


   

        460

      465 E5071CU-105 E5071CU-105E5071CU-105
      480 E5071CU-481 E5071CU-481E5071CU-481
      485 E5071CU-105 + E5071CU-486 E5071CU-105 + E5071CU-486E5071CU-105 + E5071CU-486
      4D5 E5071CU-481 + E5071CU-4D5 E5071CU-481 + E5071CU-4D7E5071CU-481 + E5071CU-4D8
      4K5 E5071CU-481 + E5071CU-4K5 E5071CU-481 + E5071CU-4K7E5071CU-481 + E5071CU-4K8



E5071C


     

        465

      460 E5071CU-205 E5071CU-205E5071CU-205
      480 E5071CU-205 + E5071CU-481 E5071CU-205 + E5071CU-481E5071CU-205 + E5071CU-481
      485 E5071CU-486 E5071CU-486E5071CU-486
      4D5 E5071CU-486 + E5071CU-4D5 E5071CU-486 + E5071CU-4D7E5071CU-486 + E5071CU-4D8
      4K5 E5071CU-486 + E5071CU-4K5 E5071CU-486 + E5071CU-4K7E5071CU-486 + E5071CU-4K8


E5071C


       480

      485 E5071CU-103 E5071CU-103E5071CU-103
      4D5 E5071CU-4D5 E5071CU-4D7E5071CU-4D8
      4K5 E5071CU-4K5 E5071CU-4K7E5071CU-4K8


E5071C


       485

      480 E5071CU-203 E5071CU-203E5071CU-203
      4D5 E5071CU-4D5 E5071CU-4D7E5071CU-4D8
      4K5 E5071CU-4K5 E5071CU-4K7E5071CU-4K8
E5071C       4D5      4K5 E5071CU-4K6 E5071CU-4K6E5071CU-4K6
E5071C       UNQ      1E5 E5071CU-1E5 E5071CU-1E5E5071CU-1E5
E5071C       019      017 E5071CU-017 (For S/N Prefix of MY461 or SG461)

 E5071CU-027 / E5071-65106

E5071CU-027 / E5071-65106
E5071C       019      017 E5071CU-027 / E5071-65106 (For S/N Prefix of MY462//3/4 or SG462/3/4)

 E5071CU-027 / E5071-65106

E5071CU-027 / E5071-65106

 1 For Win-10 units with serial prefix MY467, SG467 and newer, purchase E5071CU-390/391/392/393/394/395/396/397/2D8/2K8/4D8/4K8.
   For Win-10 units upgraded from older generation hardware (serial prefix MY461-466; SG461-466 - white color), for color matching purpose, purchase E5071CU-370/371/372/373/374/375/376/377/2D7/2K7/4D7/4K7.


Important: Above upgrades require the full adjustments and performance test. The completion of a part of calibration (adjustments and performance tests) does verify the functionality of the option, but does not guarantee that the instrument meets all published specifications. A full calibration is the only way to guarantee the analyzer specifications are being met. The upgrade labor and calibration charges needs to be quoted at the same time of the upgrade kit quotation.

3. Software Upgrades

Was this helpful?


Didn't find what you're looking for?