Do I need a keyboard and mouse to operate the X-Series Signal Analyzers?
No. However, since this is a Windows-based instrument, it is easier to navigate various windows using a mouse. Additionally, there are certain measurement applications that increase efficiency by having a mouse.
A USB keyboard can be purchased one of three ways:
- Purchasing as a model/option (N9000AK-KYB, N9000AK-KB2, N9010AK-KYB, N9010AK-KB2, N9020AK-KYB, N9020AK-KB2, N9030AK-KYB, N9030AK-KB2)
- Purchasing item number 0960-2615 (KYB equivalent) or 5188-4463 (KB2 equivalent)
-
Purchasing item number 5188-4463 (KB2 equivalent)
A USB mouse can also be purchased one of two ways:
- Purchasing as a model/option (N9000AK-MSE, N9010AK-MSE, N9020AK-MSE, N9030AK-MSE)
- Purchasing item number 0960-2616
Here are a few simple tips that can be used to navigate through the analyzer windows without a keyboard or mouse:
- Press [Menu (Alt)], [Tab] forward or backward to move between windows
- Pressing [Tab] forward or backward allows you to move from various fields within a window
- Pressing the [Arrow] keys enables parameters within a field to be selected
- Once a selection has been made, press either [Enter] key
- Press [Alt-Select] for the control menu bar
For a complete list of front panel operations refer to the Getting Started Guide or the SA Mode Help embedded in the instrument.