When using TV trigger mode with a Keysight oscilloscope, can I trigger only on even or odd fields?
Yes. All current Keysight scopes with TV triggering are capable of exclusively triggering on odd or even fields. Some models allow you to select Field 1 or Field 2 as the TV trigger source, where Field 1 corresponds to odd fields and Field 2 corresponds to even fields. See the directions below that pertain to your scope model.
5481xA, 5482xA, 54835A, 5484xA/B, 5483xB/D:
- Click Setup > Trigger
- Select the Advanced radio button and TV from the drop-down menu
- In the lower left corner, select Field 1 or 2
5462xA/D, 5464xA/D, and MSO/DSO 6000 series:
- Press the More button on the front panel
- Under the Trigger, select TV
- Press Settings
- Under the Mode, select Field1 or Field2 to trigger at the beginning of Field 1 (odd) or 2 (even). Alternatively, you can select Line:Field1 or Line:Field2 to specify a line number within the field.
DSO3000 series:
- Press Mode/Coupling
- Press Mode until Video is displayed
- Press Sync until either Odd Field or Even Field is displayed
5485xA, DSO8xx04A:
These models do not have TV trigger capability.