Is it possible to generate touchstone files on the ENA?
(SUPPORTED MODELS IN BOLD: E5071C E5072A E5070B/71B E5070A/71A E5061A/62A E5061B E5063A E5091A E5092A)
[E5071C/E5072A/E5061B]
Touchstone files can be generated by the firmware command. (Save touchstone function)
[E5070B/71B]
For the users with Firmware revision A.06.50 or later, touchstone files can be generated by the firmware command. (Save touchstone function)
For the users with firmware revision A.06.01 or older, touchstone files can be generated via the use of the "SaveToTouchstone.VBA" Visual Basic Application program.
This VBA program is installed by default as part of firmware revisions A.03.xx (and above).
[E5070A/71A]
Touchstone files can be generated on the via the use of the "SaveToTouchstone.VBA" Visual Basic Application program.
This VBA program is installed by default as part of firmware revisions A.03.xx (and above). The application will only run on firmware revisions A.02.xx and greater.
[E5061A/62A]
Touchstone files can be generated via the use of the "SaveToTouchstone.VBA" Visual Basic Application program.
This VBA program is installed by default as part of firmware.