How is the E1406A memory configured from the factory?
The E1406A ships from the factory with all the memory it can support. From the datasheet, this is 1.75 MB FLASH memory and 2 MB RAM. This memory is configured into the following 5 regions:
- FLASH - operating system
- FLASH - DSCPI drivers
- RAM (DRAM) - Driver RAM battery backed up and not cleared on power up
- RAM (NRAM) - System tables; also battery backed up and not cleared on power up
- RAM (user) - Runtime User data; cleared on power up.
When shipped from the Factory, items 3 to 5 are empty and items 2 and 3 are pre-loaded, as follows:
- alg_ctl.du supports E1415A, E1419A
- arb.du supports E1340A.
- dig_io.du supports E1330B, E1458A
- e1339a.du supports E1339A
- e1418.du supports E1418A.
- rfmux80.du supports E1470A
- scan_ad.du supports E1413A
- switch.du supports E1343A, E1344A, E1345A, E1346A, E1347A, E1351A, E1352A, E1353A, E1355A, E1356A, E1357A, E1358A, E1361A, E1364A, E1366A, E1367A, E1368A, E1369A, E1370A, E1442A, E1460A, E1463A, E1465A, E1466A, E1467A, E1468A, E1469A, E1472A, E1473A, E1474A, E1475A, E1476A, E8460A, E8462A, E8480A, E8481A, E8482A, and E8483A.
- voltmtr.du supports E1326A, E1326B, E1343A, E1344A, E1345A, E1346A, E1347A, E1351A, E1352A, E1353A, E1355A, E1356A, E1357A, E1358A, E1411A, E1411B, E1460A, E1468A, E1469A, E1476A, E8460A, and E8462A
Additional drivers can be loaded into the E1406A's RAM location. The instrument first looks in RAM for a driver before looking in FLASH. Any download of drivers into the E1406A RAM erases its contents before installing the requested drivers.
DSCPI drivers and HP-VIC are also available on the Keysight webpage at: http://www.agilent.com/find/drivers