On the ENA / ENA-L, the "Update Firmware" key is not displayed under the Service menu. What is wrong?
(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)
The Update Firmware key is not displayed because the "Initial Registration" was not performed correctly. First, perform the "System Recovery", then the "Initial Registration". The procedures for the "System Recovery" and the "Initial Registration" are described in the User's Guide and the Installation and Quick Start Guide, respectively.