Is it possible to improve the print speed of my ENA?
(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)
To improve print speed, ensure that the trigger mode is set to "trigger hold", when performing a screen dump to the printer via either the USB or parallel printer ports. Trigger hold is configured via the Trigger hard key followed by the Hold soft key.
Print speed is improved because the network analyzer CPU is optimized and dedicated for measurements. When the analyzer is configured to a "trigger hold", the CPU resources become dedicated to the printer, offering a significant reduction in print time.