What is the main reason that SMT manufacturers would use solder paste inspection for lead-free paste?
The print process for lead free requires fine tuning such as cycle time modifications, reduction in the aperature-to-pad ratios, squeegee speed/pressure changes, etc. These changes are best done with 3D solder paste inspection inspection inline because it allows for quicker print parameter optimization which saves money, time and shortens the development cycle.