How do I combine the split files that result from saving large time captures in the 35670A?
In 35670A, sometimes, when saving the time capture files onto 3 1/2 inch floppy disks, depending upon the size of the time capture buffer size, the analyzer splits the buffer data and allows for the data to be saved onto multiple floppy disks. When this situation occurs, the following is the procedure to be used to concatenate/append the data on those multiple disks to one file.
- Save the files on the multiple floppy disks containing the time capture data to
one common folder on the hard disk of the computer. - Open up the MS-DOS window and change directories to go to the folder from step 1.
- Then, execute the command: copy /B <file1>+<file2>+<file3>+.... <destination file> /V
Make sure that the order in which the data was saved from the analyzer to the multiple disks is maintained when executing the "copy" command.