How do I correct for external harmonic mixer conversion loss with a PSA Series Spectrum Analyzer (E4440A, E4446A, E4448A)?
The 11970 and 11974 series harmonic mixers supply conversion loss factor tables. The tables are in amplitude/frequency pairs. To enter these factors into your PSA press amplitude, more, corrections, user, and edit and build the table with the factors supplied. Once the table is completed, press return and turn on the corrections. Linear interpolation is used between points. Conversion loss factors are supplied on disk making loading much easier.