Starting Download..
save Save

What are the New PathWave System Design Products?

The new PathWave System Design (SystemVue) product structure is simpler and easier to configure, has fewer elements that include more application-focused value, and is your path to PathWave.

PathWave System Design Solutions

New PathWave System Design solutions enable you to:

  • Connect system-level design to RF circuit simulation
  • Verify physical layer system designs
  • Interoperate with test equipment while wireless standards evolve

What's New?

Applications

PathWave System Design - Software Bundles

PathWave System Design software bundles provide system engineers with a choice of value-packed, pre-configured combinations of software built for specific system design challenges.

Bundles

ModelProduct NameDescription
W4800BPathWave System Design CoreBase environment for PathWave System Design. Includes schematic entry, data plotting, and MATLAB code support
W4801BPathWave System Design Core + RFAdds the RF Analysis simulation element giving users access to the SPECTRASYS engine, WhatIF, linear simulation, and RF component model libraries
W4802BPathWave System Design Core + Comms/DSPA timed dataflow simulation engine to create communications and digital signal processing designs. Includes libraries of general DSP components, digital modulation, SerDes, MIMO, and legacy cellular standards
W4803BPathWave System Design Core + RF + Comms/DSPCombines both the RF and Comms/DSP analyses, allowing RF Link to connect timed dataflow analysis with accurate RF system models
W4804BPathWave System Design Core + RF + Comms/DSP + Phased ArrayAdds the advanced Phased Array Analysis simulator for both RF and Comms/DSP applications using beamforming
W4806BPathWave System Design Algorithm CoreEmbedded Algorithm Bundle - RF and Comms/DSP simulation engines for use by algorithm designers working in a MATLAB-centric environment (does not include the PathWave System Design Core component)
W4810BPathWave System Design Core + AMIHigh-Speed Digital (HSD) Bundle - Complete AMI model generation bundle. Includes the PathWave System Design Core, Comms/DSP simulator, AMI Modeling Kit, and C++ Code Generation Kit
W4811BPathWave System Design, Aerospace DefenseComplete aerospace defense system development bundle. Includes the RF, Comms/DSP, and phased array simulators as well as the Aerospace Defense Library and Visualization Kit.
W4812BPathWave System Design + 5G and CellularComplete 5G and cellular communications system development bundle. Includes the RF, Comms/DSP, and phased array simulators as well as the 5G and Cellular Library and the DPD Design Kit.
W4813BPathWave System Design, AutomotiveComplete automotive radar system development bundle. Includes the RF, Comms/DSP, and phased array simulators as well as the Automotive Library and the Ray Tracing Design Kit.
W4814BPathWave System Design + WiFi and ConnectivityComplete WiFi and Connectivity system development bundle. Includes the RF, Comms/DSP, and phased array simulators as well as the WiFi and Connectivity Library and the DPD Design Kit.
W4815BPathWave System Design + SatelliteComplete satellite communications system development bundle. Includes the RF, Comms/DSP, and phased array simulators as well as the Satellite Comms Library, 5G and Cellular Library, DPD Design Kit, and STK Link.

For more information on these bundles, refer to the PathWave System Design (SystemVue) Configuration guide.

PathWave System Design - Simulation Elements

Simulation elements are themselves comprised of one or more separate modules, which add additional design and development functions. These modules, which were formerly sold separately, are now grouped together into very efficient and effective combinations which are the bundles listed above.

Simulators

Simulators

ModelProduct NameDescription
W4501EPathWave Comms/DSP SimulationDataflow time-domain simulation engine for baseband and RF system modeling. Includes libraries of building blocks for system design including Baseband, DSP, and signal modulation
W4502EPathWave RF SimulationBring RF system modeling to your design flow with the frequency domain PathWave RF analysis simulator Spectrasys. Includes component models from RF component vendors and also the frequency planning tool WhatIF. Allows designers to use X-parameter models and RF system blocks in the time domain through RF_Link
W4503EPathWave Phased Array SimulationA powerful simulation engine for both time and frequency domain phased array creation and analysis including beamforming and antenna pattern import
W4509EPathWave System Simulation HPC 1-PackIncludes system analysis high-performance computing package for parallel computing tasks

Design Kits

Design Flow & Application Kits

ModelProduct NameDescription
W4510EPathWave DPD Design KitCapture amplifier nonlinearity and create predistortion algorithms and settings for linearization of cellular and WiFi systems
W4511EPathWave AMI Modeling KitBuild and generate IBIS-AMI models of SerDes chips and modules for use in your high-speed digital (HSD) simulations
W4512EPathWave C++ Code Generation KitCreate transportable C++ models of certain algorithmic blocks from PathWave System Design for use in other applications
W4513EPathWave Ray Tracing KitComplex environment modeling interface for automotive radar system simulation using shooting-bouncing rays (SBR) technique to capture large number of targets including independent motion. Output is used in conjunction with W4525E PathWave Automotive Library
W4514EPathWave STK LinkConnects PathWave System Design simulations to scenario models from Systems Tool Kit (STK) by AGI, Inc. enabling users to combine complex radar and electronic warfare (EW) scenarios with advanced kinematics and accurate RF system models
W4515EPathWave Aerospace Defense Visualization KitBring your radar target scenarios to life with advanced visualization to configure and quickly assess radar and target configurations prior to simulation.
W4516EPathWave 5G NR NTN Channel Model KitA satellite channel model which supports all the propagation characteristics for GEO, MEO & LEO with large path delay, large-frequency Doppler Shift, with trajectory visualization.
W4519EPathWave DPD Designer in PathWave System DesignThe W4519E is an analysis tool in PathWave System Design for architects working with digital pre-distortion (DPD). It offers compact waveforms, built-in optimized DPD analysis, a workflow with the PNA-X DPD verification capability, the new Dynamic Gain model which provides unprecedented fidelity with memory effects.

Libraries

Libraries

ModelProduct NameDescription
W4522EPathWave 5G & Cellular LibraryVerification library for all current cellular standards including 5G NR, LTE-A, and LTE. Includes reference designs and measurements for each standard, as well as MIMO channel builder capabilities
W4523EPathWave WiFi & Connectivity LibrarySimulate and verify WiFi, GPS, and Bluetooth system performance with reference sources and measurements for all connectivity system requirements
W4524EPathWave Satellite Comms LibrarySimulate DVB-x2 and GNSS signals for satellite communications systems analysis 
W4525EPathWave Automotive LibrarySimulate and verify automotive radar systems with pulse and modulation sources, target and channel models, and automotive signal processing components.
W4526EPathWave Aerospace Defense LibraryAdvanced radar simulation library including pulse signals, modulation, target, clutter, and environment models for testing radar system designs. Includes the W4514E PathWave STK Link to connect simulations to AGI's STK software.

Explorers

Explorers in ADS

ModelProduct NameDescription
W4540EPathWave DPD Explorer in PathWave ADSA new verification tool in PathWave Advanced Design System (ADS) for RF designers verifying power amplifiers with DPD at circuit level. It offers compact waveforms, built-in optimized DPD analysis, a workflow with the PNA-X model extraction and DPD verification, the new Dynamic Gain model which provides unprecedented fidelity with memory effects.

How to Buy

For more information on how you can take advantage of these powerful new software products, please consult your local Keysight PathWave Software Solutions sales representative.

Student License Program

If your studies are going online, Keysight can help. As a current user of Keysight’s PathWave Design Software, formerly Keysight EESof EDA, you are invited to make use of the student license program.

The student license program provides students and professors at supported universities fully functional licenses for use resident on their personal computer.

Send your students to get their licenses today.

For more information on how you can take advantage of these powerful new software products, please consult your local Keysight PathWave Software Solutions sales representative.

Learn more about PathWave Design Software.

Was this helpful?


Didn't find what you're looking for?