Main Support:       Knowledge Center
Documentation:   EM Design Documentation   >  Previous Supported Releases   >  EMPro 2020   >  EMPro 2020 Quick Install and License Setup   >  EMPro 2020 Quick Install-Windows

This document contains references to Agilent Technologies. Agilent's former Test and Measurement business has become Keysight Technologies. For more information, go to www.keysight.com.


Quick Install - Windows

You can install EMPro on a Windows machine after downloading the installation file from the Keysight EEsof EDA website.
                       

Obtain EMPro License File

EMPro requires a license to run. You can either apply for an Evaluation or a Purchased license. Once the license request is approved, a license file (with .lic extension) is sent as an email attachment. Save this file on your computer at C:\Program Files\Keysight\EEsof_License_Tools\bin\licenses.

Supported Platforms

For details on the Supported Platforms, refer to the Supported Platforms section.

System Requirements

The following are Keysight recommended configurations:

RAM

8 GB RAM or higher

Hard Disk Space

20 GB free disk space or greater

Processor

2.33 GHz, 64-bit, x86 quad-core processors or higher

Screen Resolution

1024 x 768

Graphical Processing Unit (GPU) Accelerator Card

For FDTD, Keysight recommends use of a Nvidia CUDA Graphical Processing Unit (GPU) accelerator card with compute capability 2.0 or greater

Download EMPro Installer

Download the latest version of EMPro.

Install EMPro

To install EMPro, you must have system administrator privileges. Run the downloaded installer (This may take a while). Follow the guided tour to complete the installation.

EMPro License Setup

At the end of installation, the License Setup Wizard starts automatically after detecting that you do not have a valid license to start ADS. If you choose to skip the license setup, you can complete the process later by selecting Start > Programs > EMPro > EMPro <release_number> > EMPro Tools > EMPro <release_number> License Manager.

Node locked License

To set up a counted license, select the Add or replace a license file option and follow the guided tour to complete the license setup process.

In case of a USB dongle, attach the dongle to the USB port and invoke the License Manager to complete your license setup.

Floating License

To set up a floating license, select the Add or replace a network license server option and follow the guided tour to complete the license setup process. Consult your license administrator for the network path of the license server. For more details on setting up floating license on a network server, see Setting Up Floating License on Windows.

Launch EMPro

To run EMPro, go to the Start menu and choose Programs >EMPro <release_number> > EMPro <release_number>




Please help us improve
Please help us improve
Was this topic helpful?