Quick Install-Linux
MBP can be installed on a Linux machine after downloading the installation file from the Keysight EEsof EDA website, as illustrated.
Obtain MBP License File
MBP requires a license to run. You can either apply for an Evaluation or a Purchased license. Once the license request is approved, a license file (with .lic
extension) is sent as an email attachment. Save this file on your computer at
$HPEESOF_DIR/Licensing/20xx.xx/linux_x86[32|64]/bin_
, where, $HPEESOF_DIR
is the product installation path.
Supported Platforms
For details on Supported Platforms, refer to the Supported Platforms section.
System Requirements
The following are Keysight recommended configurations:
RAM | Minimum 2 GB RAM recommended |
---|---|
Hard Disk Space | Minimum 1GB for a complete installation |
CPU | Minimum Single-core |
Dispaly | 1024x768 or higher |
Download MBP Installer
Click http://www.keysight.com/find/eesof-mbp-latest-downloads to download MBP.
Install MBP
To install MBP, follow the steps below:
- From a terminal (command prompt), move the
mbpxxx.xx_xxx_xxxxxxx_linux_x86.tar
file you downloaded from the Keysight EEsof EDA MBP download page (http://www.keysight.com/find/eesof-mbp-latest-downloads) to the directory you want to install MBP in. For example,mv mbpxxx.xx_xxx_xxxxxxx_linux_x86.tar /home/username/apps/
- Un-tar the installation file using the following command:
tar -xvf mbpxxx.xx_xxx_xxxxxxx_linux_x86.tar - Start the installation process using the following command:
./SETUP.SH - Once the installation finishes, add the installation directory to your
PATH
environment variable for your login.
If you are using bash shell, add the following to the end of your ~/.bash_profile or ~/.bashrc file:
export PATH=$PATH:/home/username/apps/keysight/MBP_2018/bin
If you are using C shell, add the following to the end of your ~/.tcshrc or ~/.cshrc file:
set PATH=($PATH /home/username/apps/keysight
/MBP_2018
/bin)
- Once you have added the MBP installation directory to your
PATH
, open a new terminal or logout and login again to activate the changes you made to your login's profile.
MBP License Setup
Both node-locked and floating licenses require license server to get installed and started. For a node-locked license, license server and the client machine are the same machine (that is, your local machine). For a floating license, these can be separate machines.
Keysight EEsof products no longer run on the Solaris platform; however, we still support Solaris as the license server system. |
Node-locked License
To set up a node-locked license, follow the 2-step process:
Step 1: Start License Server Managers ( lmgrd and agileesofd )
- Change the directory to the
$HPEESOF_DIR/Licensing/<license/linux_x86_[32|64]/bin
. - Run the following command to start lmgrd :
./lmgrd -c
<license file path>
-l
<license log file path>
where,- <license file path> specifies one or more full path-names to the license file(s).
- <license log file path> is the full path-name to the debug log file.
Example
./lmgrd -c /home/
userlogin
/FlexNet_Version_
x
.
x
.
x
.
x
/flexnet_
x
.
x
.
x
linux_x86_64/license.lic -l /home/_userlogin
/FlexNet_Version_
x._x
.
x
.
x
/flexnet_
x
.
x
.
x
_linux_x86_64/server_log.txt
Step 2: Set Product Environment Variable
To use a node-locked license on your machine, set the MBP_LICENSE_FILE environment variable to point to the machine running the license server managers.
To set the environment variable MBP_LICENSE_FILE in a shell, type the following commands:
csh
setenv MBP_LICENSE_FILE port@host.domain
to your ~/.tcshrc
or ~/.cshrc
file.
bash
export MBP_LICENSE_FILE=port@host.domain
your ~/.bash_profile
or ~/.bashrc
file.
Floating License
Setting up floating license on Linux is a 3-step process where both server-side setup and client-side setup are needed.
Step 1: Server-side setup
- Install Keysight EEsof EDA Licensing Software
Download and install Keysight EEsof Licensing Tools for Linux. - Start License Server Managers ( lmgrd and agileesofd )
Follow the step 1 as described in Node-locked License section.
Step 2: Client-side setup
Once the license is configured successfully for all the license servers, configure each client computer to point to the network license server. You can perform this step manually by setting up product environment variables. For details, refer to step 2 of Node-locked License Setup section.
Launch MBP
After installing MBP, add the installation path to PATH
environment variable.
Example
In bash
,
- Add
set PATH=$PATH:/home/
userlogin
/keysight/MBP_2018/bin :/home/
userlogin
/keysight/MBP_2018
in bash_profile file. - Run
mbp
in terminal to start MBP.
If you do not add the path to environment, you can use full path to launch MBP, for example, /home/
userlogin
/keysight/MBP2017/bin/mbp
and /home/
userlogin
/keysight/MBP_2018/mbp
.