Technical Overviews
SCPI Language Compatibility
X-Series Measurement App, Multi-Touch UI
N9062EM0E
SCPI Language Compatibility Measurement Application
The SCPI language compatibility measurement application transforms the X-Series signal analyzers into SCPI commands compatibility mode, by supporting over 278 SCPI commands from R&S FSP/FSU/FSE/ESU/FSV/FSL/FSW spectrum analyzers. This application enables the X-Series signal analyzers to easily replace the R&S FSP/ FSU/FSE/ESU/FSV/FSL/FSW spectrum analyzers in remotely controlled, automated test equipment (ATE) systems, with minimal or no modifications to your currently used measurement software. Figure 1 shows a simplified working block diagram for the X-Series N9062EM0E application.
X-Series measurement applications
X-Series measurement applications increase the capability and functionality of Keysight Technologies, Inc. signal analyzers to speed time to insight. They provide essential measurements for specific tasks in general-purpose, cellular communications, wireless connectivity applications, covering established standards or modulation types. Applications are supported on both benchtop and modular, with the only difference being the level of performance achieved by the hardware you select.
Top Features
The SCPI language compatibility measurement application provides an emulation process that enables the user’s legacy FSP/FSU/FSE/FSV/FSL/FSW program and X-Series signal analyzers to understand each other: Not only does this application make the X-Series understand the legacy commands for the correct implementations, it also makes the response from the X-Series signal analyzers such as measurement results and query results, understandable to the legacy remote program. By running the SCPI language compatibility measurement application, the X-Series signal analyzers support and emulate the following spectrum analyzer functions from your legacy FSP/FSU/FSE/ESU/FSV/FSL/FSW remote programs:
– General-purpose spectrum analysis settings: frequency, span, amplitude, RBW, VBW, sweep, detectors, trace averaging, data format and more
– General and delta marker functions, as well as marker noise, band power and power density functions
– Limit line and limit check functions
– Limit check for spectrum emission measurements
– Power measurements: channel power, ACP
– Statistical measurement function: CCDF
– Trace data transfer and IQ data handling
– File saving and screen copy
Refer to N9062A & W9062A SCPI Language Compatibility User Guide (literature number N9062-90001) for a complete list of compatible SCPI commands. Note: SCPI commands defined in N9062A & W9062A are 100% compatible with N9062EM0E.
Two ways to access the application
The SCPI language compatibility application emulates FSP/FSU/FSE/ESU/FSV/FSL/ FSW spectrum analyzers in SCPI programming environment only, but you can access this mode in two ways: Depending upon use cases, some of the legacy commands may not technically be possible for the emulation due to the substantial differences in the architecture and implementation between the legacy and X-Series analyzers. The SCPI language compatibility application supports commands from the spectrum analyzer mode of legacy FSP/FSU/FSE/ESU/FSV/FSL/FSW instruments, including major commands for channel power, OBW/ACP measurements, and IQ traces. Commands from other options or modes are not supported. If a command or query is valid for FSP/FSU/ FSE/ESU/FSV/FSL/FSW products but not supported by the SCPI language compatibility application, the X-Series analyzers generate an error message, indicating that this type of SCPI command is not covered in this application. The SCPI language compatibility application only emulates the FSP/FSU/FSE/ESU/FSV/ FSL/FSW spectrum analyzers in SCPI commands programming environment. It does not support the same front panel operations, user interfaces and measurement screen displays.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.