Column Control DTX

E6962A Automotive Ethernet Rx Compliance Solution

Data Sheets

Introduction

The Keysight E6962A automotive Ethernet Rx validation and conformance application provides you with an easy and accurate way to verify and debug the receiver characteristics of your BroadR-Reach and 100BASE-T1 designs.

Next-generation ADAS systems require camera and radar systems with increasingly high resolution.That means new requirements for speed and bandwidth—and automotive Ethernet provides much faster transfer of ADAS-related data.Automotive Ethernet enables faster data communication to meet the demands of today’s vehicles and the connected vehicles of the future.Unlike the slower speed backplanes of CAN and LIN, 100BASE-T1 Automotive Ethernet requires rigorous compliance testing.Keysight’s full suite of automotive Ethernet solutions automate testing and validation across Tx, Rx and link segment for 100 Mb/s or 1000 Mb/s automotive Ethernet.

The E6962A automotive Ethernet Rx test software lets you automatically execute Ethernet physical-layer (PHY) electrical tests for receiver compliance using IEEE 802.3bw.The E6962A displays the results in a text report format.In addition to the measurement data, the report includes BER measurement and pass/fail limits.

The E6962A automotive Ethernet Rx test software performs complete BER count to ensure the DUT can maintain a BER of less than 10-10 and meet the OABR BroadR-Reach V3.2 specification.To meet signal quality requirements, your product must successfully pass conformance testing against these standards.Performing this test is not only required but will give you confidence in your design.The Keysight E6962A BroadR-Reach Rx application will save you hours of valuable time with automatic configuration, instrument setup, calculations and report generation.

Using the Keysight E6962A BroadR-Reach RX Compliance Application (100BASE-T1 compliant) software greatly simplifies BroadR-Reach receiver compliance testing.The software automati­cally configures the required test equipment, reducing the overall test time.

The E6962A BroadR-Reach Rx compliance application is available in the following license variations.

E6962A-1FP BroadR-Reach Rx compliance application, fixed perpetual license

E6962A-1TP BroadR-Reach Rx compliance application,transportable perpetual license

 

Note: The software is installed and runs on a Keysight PXI embedded controller and works with Keysight PXI AWG/Digitizer module

Features

The BroadR-Reach Rx compliance software offers several features to simplify the validation of automotive Ethernet designs:

The E6962A Software:

Guides you how to make connections to the device under test.

Automatically checks for proper configuration.

Automatically sets up the test equipment for each test.

Provides detailed information of each test that has been run.

Creates a printable text report of the tests that have been run.

 

E6962A BroadR-Reach Rx compliance software

The E6962A BroadR-Reach Rx test software saves you time by setting the stage for automatic execution of 100BASE-T1 BER test.Some of the difficulties in performing the BER test for 100BASE-T1 are: properly understanding the specification, configuring/ running the instrument/s and then analyzing the measured results by comparing them to limits published in the specification.The E6962A 100BASE-T1 electrical test software does much of this work for you.

The E6962A BroadR-Reach Rx test software automatically configures the PXI modules for the test and provides an informative results report that includes a BER measurement and a pass/fail limit.See Table 1 for a list of the measurements and specifications tested in the E6962A.

E6962A Software saves you time

It can be difficult to build the bit error rate verification system to characterize the Rx signals and get an accurate BER count.Keysight takes the complexity away and offers a clear validation of the BER count objectively.This saves you time and hassle in under­standing the specifications, setting up the tests and interpreting the results.

The E6962A BroadR-Reach Rx test software extends Keysight’s PXIe modular equipment to do a complete BER count.The Keysight E6962A quickly walks you through the steps required to set up the tests, perform the tests, and view the results.
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
By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX