Technical Overviews
Banded Measurement Solutions to 1.5 THz
Keysight offers a variety of banded millimeter-wave solutions that enable Keysight network analyzers to make component measurements up 1.5 THz. These four solutions are easily configurable with frequency extenders from Virginia Diodes Inc.
Supported solutions through Keysight may be configured with or without a test set controller, depending on the measurements required and the frequency extenders being used.
High performance solutions with PNAs
1. PNA test set controller configuration: N522xB/4xB PNA/PNA-X with N5292A test set and N5256/62 frequency extenders
2. PNA direct connect configuration: N522xB/4xB PNA/PNA-X with N5256/62 frequency extenders
Affordable solutions with Streamline or PXI VNAs
For higher measurement performance, frequency offset or other measurement applications, the PNA/-X based banded configuration is required.
3. USB/Thunderbolt Streamline or PXI VNA with N5252APXI test set configuration: P93xxA/B and P50xxA/B Streamline VNA or M937xA/M980xA PXI-VNA with N5262BW frequency extenders and N5252APXI test set (frequency extender adapter) up to WR 3.4 bands (P937xA or M937xA can be used up to D-band).
4. USB/Thunderbolt Streamline or PXI VNA direct connect configuration: P93xxA/B and P50xxA/B Streamline VNA or M937xA/M980xA PXI-VNA with N5252AW frequency extenders for V, E, W and D bands.
Supported measurement capability
You can make S-parameters, power measurement and sweep 8, and antenna measurements with both test set controller and direct control configurations. This table is a summary of available measurement application software. (S93xxxB/S94xxxB that are not on this list are not supported.)
PNA Test Set Controller Configuration
Key features
PNA Test Set Controller Configuration
Test set controller based solutions performance
The test set controller based solutions offer not only the highest frequency coverage up to 1.5 THz but have also shown the best dynamic range in the industry.
The following is an example of a WR2.2 frequency extender dynamic range using a PNA/PNA-X network analyzer, and a N5262A test set controller with a typical performance of 100 dB in a 10 Hz IFBW.
Ease-of-use
The banded millimeter-wave system uses built-in firmware, allowing you to leverage the built in software features of the PNA and PNA-X Series network analyzers.
Regardless of the frequency range of your measurements, you can manually control the instrument from the front panel or use a mouse to access the simple pull-down menus.
In addition, you can utilize Cal Wizard to guide you step-by-step through the most complicated of calibrations.
The banded millimeter-wave system can easily be configured using the dialogue box shown in Figure 2. Multiple system configurations can be added to the list, but only one is active at a time.
Creating a banded configuration is easy, simply enter the start and stop frequencies and the multipliers for RF and LO frequency ranges (the values are located on the test head modules).
Once a configuration has been added to the list, simply highlight the setup of choice and then click Activate Selected Config to apply.
PNA Direct Connect Configuration
These solutions do not require a millimeter-wave test set controller as they connect directly to the front panel of a dual source PNA or PNA-X. VDI frequency extenders are supported with this configuration.
Here is an example of a set of VDI modules that are directly connected to a dual source PNA.
Key features
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.