How should I setup M9485A for the non-Keysight chassis?
Setup for Non-Keysight PXI Chassis
When you use Non-Keysight PXI chassis for the M9485A, the routing setup for trigger is required. The following figures show the required trigger routing.
Configuration A (installed from slot 2 for up to 6 receivers)
Configuration B (installed from slot 2 for 7 to 12 receivers)
Configuration C (installed from slot 8 for up to 6 receivers)
Setup Example for NI PXIe-1075 & PXIe-1085
1. Launch NI-MAX.
2. Select NI PXIe-1075 or NI PXIe-1085.
3. Select "Routing" as pictured below.
Configuration A (installed from slot 2 for up to 6 receiver)
Configuration B (installed from slot 2 for 7 to 12 receivers)
Configuration C (installed from slot 8 for up to 6 receivers)
4. Press "Save".
About Ext Trig in
Master Receiver Module Trig-In Port (Front Panel) is supported as External Trigger In.
Multi-Chassis Support
Multi-Chassis is not supported for Non-Keysight PXI Chassis.