Starting Download..
save Save

How do I upgrade my N9000B CXA Signal Analyzer?

Most all of the N9000B options that are sold at the time of instrument purchase are also available as an upgrade option.  Upgrade options can vary from a simple license key installation to more complex upgrades that involve installling multiple pieces of hardware. For each upgrade option it is advised that each row in the table is read and understood. Before purchasing an upgrade option that contains hardware items, the following steps should be taken:
 

  1. View the installation note by selecting the Install Note link in the Upgrade Contents cell. 
  2. Determine from the installation instructions the complexity of the installation and whether you will perform the upgrade yourself or have a Keysight Service Center perform the installation. 
  3. Review the Utilities, Adjustments & Performance Verification Tests section of the installation instructions to see what the required adjustments and performance tests are once the upgrade is installed. 
  4. Review the following lists of test equipment requirements for each required adjustment and performance test to further determine whether you have the ability to perform the upgrade yourself or have an Keysight Service Center perform the installation.

If an upgrade option is going to be installed by a Keysight Service Center, additional labor charges may apply. Your Keysight field engineer can provide an all inclusive quote for this.

All instrument adjustments are automated and require the use of the Keysight Performance Verification & Adjustment Software.

Many hardware upgrades will require the redemption and installation of a license key file (.lic) to activate the option. Once a redemption certificate is received the license key file can be redeemed at the Keysight Software License Redemption Website

N9000B Internal Hardware Options

OptionDescriptionOrder AseDeliveryUpgrade ContentMinimum FirmwareAdjustments Required1Additional RequirementsIncompatible WithInstalled ByInstallation Time
B25

25 MHz Analysis Bandwidth

N9000BU-B25

Yes
  1. Install Note
  2. Entitlement Certificate
NoneNoNoneNoneService Center Recommended3

Install=0.5 Hrs
Adjust & Verify=0.5 Hrs

EDPEnhanced Display PackageN9000BU-EDPYes
  1. Install Note
  2. Entitlement Certificate
NoneNoNoneNoneUserInstall=0.5 Hrs
Adjust & Verify=0.0 Hrs
EMCBasic Precompliance EMI FeatureN9000BU-EMCYes
  1. Install Note
  2. Entitlement Certificate
     
NoneNoNoneNoneUserInstall=0.5 Hrs
Adjust & Verify=0.0 Hrs
ESCExternal Source Control FeatureN9000BU-ESCYes
  1. Install Note
  2. Entitlement Certificate
  3. Hardware
     
NoneNoNone513, 526UserInstall=0.5 Hrs
Adjust & Verify=0.0 Hrs
FSAFine Resolution Step AttenuatorN9000BU-FSAYes
  1. Install Note
  2. Entitlement Certificate
     
NoneYesNoneNoneService Center Recommended3

Install=0.5 Hrs
Adjust & Verify=3.0 Hrs

P03Preamplifier, 3 GHzN9000BU-P03Yes
  1. Install Note
  2. Entitlement Certificate
     
NoneYesNoneP07, P13, P26Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

P07Preamplifier, 7.5 GHzN9000BU-P07Yes
  1. Install Note
  2. Entitlement Certificate
     
NoneYesNone503, P13, P26Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

P13Preamplifier, 13.6 GHzN9000BU-P13Yes
  1. Install Note
  2. Entitlement Certificate
     
NoneYesNone503, 507, P26Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

P26Preamplifier, 26.5 GHzN9000BU-P26Yes
  1. Install Note
  2. Entitlement Certificate
     
NoneYesNone503, 507, 513Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

PC7SCPU/SSD assembly with on-board calibration data memoryN9000BU-PCSNo
  1. Hardware
  2. Install Note
A.25.08
Firmware pre-installed on SSD
 

No
(if existing cal data can be backed up)

See Install Note link

None


SSD includes Win 10

Windows 7Service Center RecommendedInstall=1.0 Hrs
Adjust & Verify=0.0 Hrs
 
PFRPrecision Frequency ReferenceN9000BU-PFRYes
  1. Install Note
  2. Entitlement Certificate
     
NoneYesNoneNoneService Center Recommended3

Install=0.5 Hrs
Adjust & Verify=1.0 Hr

SF1Security Features, Exclude Launching ProgramsN9000BU-SF1Yes
  1. Install Note
  2. Entitlement Certificate
     
NoneNoNoneNoneUserInstall=0.5 Hrs
Adjust & Verify=0.0 Hrs
SF2Security Features, Prohibit Saving ResultsN9000BU-SF2No
  1. Install Note
  2. Entitlement Certificate
     
NoneNoNoneNoneService Center RecommendedInstall=1.0 Hrs
Adjust & Verify=0.0 Hrs
SSDWindows Embedded Standard 7 Solid State Drive N9000BU-SSDNo
  1. Hardware
  2. Install Note
  3. Software
NoneNo2NoneNoneService Center RecommendedInstall=0.5 Hrs
Adjust & Verify=0.5 Hrs
T03Tracking Generator, 3 GHzN9000BU-T03No
  1. Hardware, License Key
  2. Install Note
NoneYesNone513, 526Service Center RecommendedInstall=1.0 Hrs
Adjust & Verify=2.0 Hrs
 
T06Tracking Generator, 6 GHzN9000BU-T06No
  1. Hardware, License Key
  2. Install Note
NoneYesNone503, 513, 526Service Center RecommendedInstall=1.0 Hrs
Adjust & Verify=2.0 Hrs
 
W10Windows 10 Solid State Drive N9000BU-SS1No
  1. Hardware
  2. Install Note
  3. Software
NoneNo2PC7NoneAdvanced User Install=1.0 Hrs
Adjust & Verify=0.0 Hrs
 

 

N9000B External Hardware Options

OptionDescriptionOrder AseDeliveryUpgrade ContentMinimum FirmwareAdjustments Required1Additional RequirementsIncompatible WithInstalled ByInstallation Time
1CM113ARackmount Kit (Rack Flanges Only)1CM113ANo
  1. Hardware
  2. Install Note
NoneNoNonePRC, 1CN103A, 1CP105AUserInstall=0.5 Hrs
1CN103AFront Handle Kit (Handles Only)1CN103ANo
  1. Hardware
  2. Install Note
NoneNoNonePRC, 1CM113A, 1CP105AUserInstall=0.5 Hrs
1CP105ARack Mount Kit with Handles1CP105ANo
  1. Hardware
  2. Install Note
NoneNoNonePRC, 1CM113A, 1CN103AUserInstall=0.5 Hrs
1CR013ARack Slide Kit (Rack Slides Only)1CR013A or E4406-60115No
  1. Hardware
  2. Install Note
NoneNoNonePRCUserInstall=1.0 Hr
1DVR001AUSB DVD-ROM/CD-R/RW Drive1DVR001A or 0950-5369No
  1. Hardware
NoneNoNoneNoneNot applicableNot applicable
1KYB001AUSB Keyboard - Compact1KBD001A or 0960-2929No
  1. Hardware
NoneNoNoneNoneNot applicableNot applicable
MLP001AMinimum Loss Pad, 50-to-75 OhmsMLP001A or 0955-1020No
  1. Hardware
NoneNoNoneNoneNot applicableNot applicable
1MSE001AUSB Mouse1MSE001A or 0960-2670No
  1. Hardware
NoneNoNoneNoneNot applicableNot applicable
PRCPortable ConfigurationN9000BU-PRC
 
No
  1. Hardware
  2. Install Note
NoneNoNone1CM113A, 1CN103A, 1CP105A, 1CR013AUserInstall=1.0 Hr

1 While the completion of the recommended adjustments and performance tests for a given option upgrade does verify the functionality of the option, it does not guarantee that the entire instrument meets all published specifications. A full instrument calibration is the only way to guarantee that all instrument specifications are being met.
2 The instrument calibration data file MUST be transferred in order for the analyzer to meet specifications. If the cal file is not transferred all adjustments and performance tests must be performed. Refer to the Installation Note for details.
Upgrade can be performed by the User without any performance verification required if the instrument being upgraded is still within it's original factory calibration cycle and no major repairs or adjustments have been performed on it. See the upgrade installation note for more details.

Instrument Software:

Instrument Software Update:

The software update package for the X-Series Signal Analyzers contains the spectrum analyzer measurement application, all the advanced measurement application software, and all other updates required by the individual measurement assemblies inside the instrument.

Keysight recommends updating the instrument software version whenever an internal hardware upgrade or measurement application is installed into the analyzer.

The latest revision of the instrument software installer can be found at:

Measurement Applications:

To see the complete list of software measurement applications available for the N9000B Signal Analyzer, see:

Measurement Applications require the redemption and installation of a license key file (.lic). Measurement application upgrades are meant to be performed by the customer, and no adjustments or performance verification tests are required.

In order to redeem a license key, the end user must have a valid redemption certificate and then go to the Keysight Software License Redemption Website.

Available Accessories:

Was this helpful?


Didn't find what you're looking for?