What specification adder should be applied when performing Ohms measurements with OCOMP off?
The instrument's published specifications apply equally for OCOMP ON and for OCOMP OFF measurements. OCOMP ON automatically performs the equivalent of a "reversal" measurement to remove the external error created by offset voltages present in the users' cabling, connections or resistor under test. The user is responsible for eliminating or accounting for these non-instrument errors when performing high-accuracy Ohms measurements with OCOMP OFF.