Which 34980A Switch Modules are supported by the IviSwtch api?
The following modules are SUPPORTED by the IviSwtch API of the 34980A IVI driver:
- 34921A
- 34922A
- 34923A
- 34923A-1W
- 34924A
- 34925A
- 34925A-1W
- 34931A
- 34932A
- 34933A
- 34933A-1W
- 34934A-4x32
- 34934A-4x64
- 34934A-4x128
- 34934A-8x32
- 34934A-8x64
- 34934A-16x32
- 34937A
- 34938A
- 34939A
- 34941A
- 34942A
- 34946A
- 34947A
The following modules are NOT SUPPORTED by the IviSwtch API, but can be accessed using the Ag34980a specific driver:
- 34945A
- 34950A
- 34951A
- 34952A
- 34959A
Last Revised: January 21, 2014 - driver version 1.5.3.0