How do I figure out the analysis bandwidth upgrade option(s) I should order to achieve the analysis bandwidth I need to have in my X-Series analyzer?
Today's complex measurements and modulation schemes are requiring wider analysis bandwidths. In order to achieve these wider bandwidths in a signal analyzer, specific options are required. The X-Series analysis bandwidth wizard tool will help end user customers determine the exact upgrade option(s) that should be ordered to achieve the analysis bandwidth that is needed to make their complex measurements.
The end user simply needs to select their product, desired analysis bandwidth (e.g. 160 MHz), current bandwidth (e.g. 25 MHz), frequency option, and specific installed option information. After making these selections, the wizard will display the upgrade options that are required to achieve the desired analysis bandwidth. Find out which upgrade option(s) you need by using the Bandwidth Upgrade Wizard
The installation of analysis bandwidth upgrade options vary in complexity depending on the options that currently exist in the analyzer. Once the upgrade options are determined, it is highly recommended that you refer to the X-Series upgrade webpages to determine the level of complexity for each upgrade option that is needed. The links below will take you to the appropriate product upgrade webpage: