Will Windows 7 work on my existing processor?
Similar to PC’s, there is a minimum configuration/vintage of processors which are compatible with Windows 7 and these are denoted as PC4/PC5/PC6/PC7 in the show system screen on your instrument. Upgrades to these latest processors are available which take advantage of more memory as well as Windows 7 functionality.
To find out which processor you have and what type of upgrade option you will need to get you where you want to be, select the "What upgrade options do I need to order if I want to update my operating system..." found in Documents & Downloads.