Can the B2961A/B2962A step the source value immediately after the value is changed by its rotary knob?
In the default setting, the source value becomes effective on the B2961A/B2962A after setting the value and fixing it by the operation such as pressing the rotary knob, the assist keys, etc. At that moment, the status changes to MOVE (blue).
However, once Immediate V/I Update function is enabled, the output will be stepped whenever you change the source value by rotary knob even in the EDIT (green) status.
Please see the following material for the details.
How to enable Immadiate V/I Update function on B2961A/B2962A