How do I create a waveform sequence on the 33500B Series waveform generators?
Sequences can only be created remotely. Once a sequence is created and stored on the 33500A and 33500B Series models in the form of a .seq file, it can be downloaded from the instrument using a memory stick / USB flash drive. The .seq file can then be opened on a computer using a text editor and changed to create a different sequence. The file can then be uploaded to the waveform generator as a new sequence.