Column Control DTX

Strain-Rate Sensitivity of Nickel by Instrumented Indentation

Application Notes

In many materials, the plastic stress that can be sustained depends on strain rate through a power-law relationship: higher stresses are sustained with higher strain rates and vice versa. In a uniaxial tensile configuration, this relationship between plastic stress, s, and strain rate, e•, is expressed as


where B* is a constant and m is the strain-rate sensitivity (SRS), which is always greater than or equal to zero. For materials which manifest negligible strain-rate sensitivity, m is near zero, making s a constant. (Sapphire is an example of such a material.) Materials with greater strain-rate sensitivity have greater values of m. 

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX