I cannot store the channel 2 measurement condition to USB memory stick, why not?
Question:
I cannot store the channel 2 measurement condition to USB memory stick. Why?
Answer:
The instrument may be configured to use the conventional command set designed for using the existing programs which you created to control existing instruments such as Keithley 2400.
It allows the users to use the channel 2 only with front panel operation as long as the operation doesn’t conflict with Keithley 2400 SCPI commands. So you can set up the channel 2 condition with front panel operation even if the instrument is configured to use the conventional command set.
However, the condition for the channel 2 can’t be saved to USB memory. Only the condition for the channel 1 can be saved.
Please take the actions described in the material below and configure the instrument to use the default command set which supports all the B2901/02/11/12A functions.