How do I upgrade my handheld spectrum analyzer?
Most of the upgrades to the HSA can be made by obtaining a license key and do not require hardware installation. The tracking generator, Option TG7, is one upgrade which requires the installation of hardware. Firmware upgrades can be made by the user via a USB port or LAN port.
For the upgrades available for a specific model , please refer to the links.