Can I use Command Expert when I don't have an actual instrument?
Yes. Command Expert lets you work offline with instruments. Working offline is a simulation mode in which you can view and perform commands as usual, but all commands return default outputs. This is a good way to explore a command set, view documentation and prototype command sequences before you have the physical instrument.
Command Expert 1.2 allows you to specify an IO Monitor log file file in place of an instrument address. Command Expert will parse the log file and match responses to commands found in your sequence. This will allow you to playback a sequence with real simulation.
Last Revised April 28th, 2013