Starting Download..
save Save

How Do Recalibrate the FieldFox Battery Pack?

FieldFox battery pack is a smart battery, which has a built-in monitoring system to check the accuracy of the charge gauge. From the FieldFox battery display view, if the Max Error is 10%, it is recommended to recalibrate the battery pack using external battery charger, N9910X-872. This will recalibrate the accuracy of the battery's charge gauge.

For more information about Fieldfox handheld RF and microwave analyzer, please visit FieldFox Handheld RF and Microwave Analyzers.

Was this helpful?


Didn't find what you're looking for?