What is the measurement range operation used with pulsed output?
When you specify the pulsed output, AUTO measurement range mode becomes unavailable.
Even if you specify AUTO measurement range operation with the pulsed output, FIXED measurement range operation is used internally.
In this case, the measurement range is selected based on Limit (compliance) value. for example, if you specify 20 mA limit value, 100 mA current meassurement range is used.
If you specify FIXED measurement range operation with the pulsed output, B2901/02/11/12A uses the specified measurement range with FIXED range operation.