What file types can be shared between versions of 89600 VSA software?
This table list all the major file types accessed by 89600 VSA software. A checkmark indicates that the functionality listed at the top of the column is available for the file type.
File Type | Write from version 12.xx | Read to version 12.xx | Write from version 13.00 or greater | Read to version 13.00 or greater |
---|---|---|---|---|
Setup (.set) | ||||
Setup (.setx) | ||||
Recording (.sdf, .csv, .txt, .mat, .hdf, .h5, .bin, .cap, .dat) | ||||
Trace (.sdf, .csv, .txt, .mat, .hdf, .h5, .dat) | ||||
Limit Line (.lim) | ||||
Limit Test (.lims) | ||||
Math (.mth) | ||||
Math (.mthx) | ||||
User Color Map (.ucm) | ||||
State Definitions (.csd) | ||||
Demo (.htm) | ||||
VB Script Macro (.vbs) | ||||
C# Macro (multiple files) | ||||
VB.Net Macro (multiple files) | ||||
OFDMA Map (.omf) | ||||
User IF/RF Calibration (.cal) | ||||
Arbitrary Waveform (.arb) | ||||
Display Appearance (.dap) | ||||
Display Preferences (.dspx) | ||||
Layout (.layx) |