Configuration Guides
Configuration Guide
See Through the Complexity
Development becomes more complex when faster data rates intersect with today’s crowded spectral environment. Finding a signal problem is essential—but achieving the clarity to pinpoint the answer is the crucial challenge.
PathWave Vector Signal Analysis (VSA) software is a comprehensive set of tools for demodulation and vector signal analysis. These tools enable you to explore virtually every facet of a signal and optimize your most advanced designs. As you assess the tradeoffs, PathWave Vector Signal Analysis (VSA) helps you see through the complexity.
Configure Your New Software
This step-by-step process will help you configure your new PathWave Vector Signal Analysis (VSA) software when making your initial order. See the upgrade section to learn how to add any of these options after initial purchase.
Step 1: Choose Basic Vector Signal Analysis
Step 2: Add Other 89600 VSA Measurement Applications
Step 3: Select Desired License Type, License Term and Subscription
Each of the following license types are offered as perpetual or subscription licenses as shown in the table below. A valid support contract is included with subscription licenses. For perpetual license, a separate support contract is required to access Keysight technical support and software updates.
Step 4: Confirm 89600 VSA Ordering Information
Configuration Example
In this example with 89601C, 5 people can use the 89601C VSA software at the same time because of quantity of 5 option 89601200C floating licenses have been purchased.
This means that at any one time, two users can make LTE/LTE-A FDD measurements because two LTE/LTE-A FDD option 89601BHGC licenses have been purchased, three users can make 5G NR measurements because one 5G NR option 89601BHNC license has been purchased, and two more users can use 89601C VSA software to make basic time and spectrum measurements (without LTE/LTE-A FDD or 5G NR).
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.