Column Control DTX

Convert Tescon Point 70 Fixtures for Use on i1000D ICT System

Application Notes

Introduction to Medalist i1000D

The Keysight Technologies, Inc. Medalist i1000D in-circuit test (ICT) system is a revolutionary platform targeted for maximum cost effectiveness. It offers award winning stateof-the-art features with answers to most test challenges faced by today’s manufacturers. Advanced defects coverage features coupled with a simplified software model shorten the learning curve of new users, making this an ideal investment for manufacturers who need a cost effective ICT solution. It’s back to the basics with the Medalist i1000D software to help new users get up to speed in the shortest time possible.

Following the development model of a typical manufacturing defects analyzer (MDA), the user can now get a fixture and program up and running in just a few days. Simplified graphical user interfaces allow the user to quickly make changes to individual tests during debug, with a comprehensive toolset of menus and buttons complete with AutoDebug features. This allows inexperienced users to start using the system quickly.

The purpose of this application note is to guide users on how they can convert both the hardware and software systems of their old Teson MDA platform over to the Medalist i1000D platform so as to enjoy the capabilities offered by the i1000D ICT system. 

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX