Column Control DTX

E1738A Air Temperature/Pressure/Humidity Sensor

Data Sheets

 The E1738A Air Sensor is used with the Keysight E1736A USB Sensor Hub as part of the 5530 Laser Calibration System. The E1738A Air Sensor connects to the E1736A USB Sensor Hub via a detachable E1739A/B/C/D sensor cable. Sensor cables come in different lengths (5 m, 10 m, 15 m, 25 m), they have easy snap-on connectors so users can quickly change cable lengths as needed.

The E1738A Air Sensor monitors the air in the environment of the measurement to enable the laser calibration system to automatically adjust for the changes to the laser wavelength. The sensor has a magnetic base for ease of attachment.
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
By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX