Starting Download..
save Save

How do I upgrade my N9330B Handheld Cable and Antenna Tester?

 Most of the N9330B Handheld Cable and Antenna Tester options are available for post-sale retrofit.

Measurement Personalities are application specific and may require additional hardware or accessories.

Basic hardware upgrades kits contain installation instructions and the desired assembly. Other hardware upgrades require the instrument to be taken apart for the upgrade to be added to the instrument. Adjustments or performance verifications are then required to ensure the instrument meets the published specifications. The instrument may need to be shipped to an Keysight Service Center to have the upgrade installed. Make sure to obtain a quote for the installation before bringing the instrument and upgrade kit to a Keysight Service Center to get installed.

The table below provides the necessary Installation Note for each upgrade. The installation note includes a list of the performance verification tests and adjustments required as well as the test equipment and test software necessary to complete the upgrade. Performing the tests listed in the installation note guarantees the newly installed option is functioning, but a full instrument calibration is the only way to guarantee specifications are being met.

Some upgrades may require that a minimum firmware is already installed. Up-to-date firmware can be downloaded for free from the N9330B Firmware Update Center.

Some upgrades may also require the redemption and installation of a license key before they will be activated. Once a redemption certificate is received, the license key(s) can be redeemed at the Software License Redemption Web Site.

Option Description Order As Installation Note Upgrade Contents Minimum Firmware Adjustments Required Additional Requirements Incompatible With Installed By - Installation Time
1DN Automotive 12V DC Charger N9330BK-1DN None  Hardware None No None None Customer - 0.0 Hrs
1TC Hard Transit Case N9330BK-1TC None Hardware None No None None Not applicable
201 Mechanical calibrator, 50ohm, DC-4GHz, male N N9330BK-201 None Hardware None No None None Customer - 0.0 Hrs
202 Mechanical calibrator, 50ohm, DC-4GHz, male 7/16 DIN N9330BK-202 None Hardware None No None None Customer - 0.0 Hrs
203 Electronic Calibrator N9330BK-203 None Hardware None No None None Customer - 0.0 Hrs
301 Extension cable, male N to female N, 1.5 m N9330BK-301 None Hardware None No None None Customer - 0.0 Hrs
302 Extension cable, male N to female 7/16 DIN, 1.5 m N9330BK-302 None Hardware None No None None Customer - 0.0 Hrs
303 N (M) to 7/16 DIN (F) Adaptor N9330BK-303 None Hardware None No None None Customer - 0.0 Hrs
304 Extended cable 1.5 m N (male) – 1N (male) N9330BK-304 None Hardware None No None None  Customer - 0.0 Hrs
AB2 Simplified Chinese printed User's Guide N9330BK-AB2 None User's Guide None No None None Not applicable
ABA English printed User's Guide N9330BK-ABA None User's Guide None No None None Not applicable
ABJ Japanese printed User's Guide N9330BK-ABJ None User's Guide None No None None Not applicable
ADP Spare AC/DC adaptor (for countries not listed for AUS) N9330BK-ADP None Hardware None No None None Customer - 0.0 Hrs
AUS Spare AC/DC adaptor for United States, Canada, China, Mexico, Argentina, Australia/NZ, Taiwan N9330BK-AUS None Hardware None No None None Customer - 0.0 Hrs
BAT Battery Pack N9330BK-BAT None Hardware None No None None Customer - 0.0 Hrs
BCG External Battery Charger N9330BK-BCG None Hardware None No None None Customer - 0.0 Hrs
PWM Power Monitoring (USB power sensor not included) N9330BK-PWM None License key ≥ B.01.15 No None None Customer - 0.5 Hrs
Was this helpful?


Didn't find what you're looking for?