PCIe 2.0 PTC required tests for PCI-SIG compliance testing ========================================================== This is a package containing test code for the E2969B PTC-II card from Agilent Technologies. It contains all required tests that the PCI-SIG will test during its compliance workshops, using this Agilent hardware. This is to qualify for the PCI Express 2.0 Integrators List. To install this required package, please follow these steps: - Please read the file "version.txt" for information on compliance of this package with full Agilent software packages for E2960B family. - Download and install the latest full Agilent software version that is mentioned in the "version.txt" file, by going to http://advanced.comms.agilent.com/spt/downloads/download.htm - Make sure the Agilent software for Protocol testers is not running. - Run the .EXE file that comes with this PTC package. It is a self-extracting executable. In the "Unzip to folder" option it should show "C:\" . Please don't change this! - After you installed this package, please run the "Firmware Update" utility from the "Agilent System Protocol Tester" program group while your E2969B hardware is running and connected through USB. This will ensure the necessary firmware that is compliant to this PTC package is programmed into your hardware. Otherwise an update will be requested by this utility. For any questions, please contact Agilent Support, at dvs-spt_support@agilent.com