Configuration Guides
Introduction
This demonstration guide helps you to get familiar with the basic setup and configuration requirements to perform power measurements using the Keysight Technologies, Inc. U2000 Series USB power sensor via
Keysight N1918A Power Analysis Manager.
All demonstrations exercised in this guide require the U2000 Series bundled application software N1918A Power Analysis Manager–Power Panel, any of the U2000 Series USB power sensors and a Keysight ESG E4438C vector signal generator.
This demonstration guide includes a step-by-step demonstration of basic average and pulse measurements.
Power Panel
The Power Panel is the basic version of the Power Analysis Manager and is bundled with the purchase of a U2000 Series USB power sensor. The Power Panel provides an easy-to-use GUI that offers basic features that can be found in a typical power meter.
Key Features
U2000 Series USB Power Sensors
The U2000 Series USB power sensors are average, wide dynamic range power sensors that can be used with a PC or any selected Keysight USB-based instrument.
Key Features
Demonstration Preparation
The following instruments and software are required in order to perform the demonstrations illustrated in this demo guide:
Instructions
Pulse Power Measurement Demonstration
Pulse power is determined by measuring the average power of the pulse and then dividing the measurement results by the pulse cycle value to obtain the pulse power reading, as expressed by the following equation:
Pp = Pavg / Duty Cycle
The measurement result is a mathematical representation of the pulse power rather than the actual measurement with the assumption of constant peak power. To ensure accurate pulse power readings, the input signal must be a repetitive rectangular pulse with a constant duty cycle.
Objective
To demonstrate the capability of the Power Panel to carry out pulse power measurement using the U2000 Series USB power sensor.
In this demonstration, we supplying a pulsed signal with the pulse width of 10 μs and a pulse period or pulse repetition interval (PRI) of 40 μs. The pulse signal is set to the power level of approximately 0 dBm. The measured average power of the signal is –6.24 dBm (See Figure 6). The duty cycle is known to be 10 μs divided by 40 μs, which is 25%—this value can be configured in the Power Panel. This generates a pulse reading of –0.22 dBm (See Figure 7).
To understand what the USB power sensor does, we can look at the duty cycle calculation. The equation, Average Power = 10 log (Pulse Width/PRI), provides the difference between average power and pulse power. The calculated value in this demonstration shows that the average power is –6.02 dBm lower than the pulse power. The Power Panel makes this correction to show the pulse power using the provided duty cycle.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.