Is there a sample file of the MWA software that I can customize for my DUT?
(SUPPORTED MODELS IN BOLD: E5071C E5072A E5070B/71B E5070A/71A E5061A/62A E5061B E5063A E5091A E5092A)
Yes, csv files that contain all setup parameters for example devices can be downloaded below. Refer to the setup procedure of the MWA software for each device and customize parameters with the MWA front-end application for your own devices.
How to import a csv file by the MWA front-end application
Step 1. Launch the MWA front-end application ("mwa_xxxx.xls"). The latest revision of the MWA front-end application can be downloaded at: https://www.keysight.com/find/mwa
Step 2. Select the System sheet in the front-end application.
Step 3. Import a csv file by selecting "Import Data..." in the sheet.
You can change any setup parameters for your DUT with the MWA front-end application.
How to generate a setup file for the MWA (*.mwa)
Step 1. Select the Output sheet in the front-end application.
Step 2. Click on "Save Spec Sheet" in the sheet.
List of MWA files for sample devices
Device Example | Number of Port | Setup Procedure | Setup csv file | Comment |
---|---|---|---|---|
3-port BPF | 3 | *.csv | Without using a multiport test set. | |
SP9T Switch | 10 | *.csv | Using 10-port full crossbar configuration of the E5092A. | |
Balanced Cable | 16 | *.csv | Using 16-port full crossbar configuration of the two E5092As. | |
Multiple 2-port DUTs | 2 x 11 | *.csv | Using 22-port configuration of the E5092A. | |
Multiple 3-port DUTs | 3 x 7 | *.csv | Using 22-port configuration of the E5092A. | |
Multiple 4-port DUTs | 4 x 5 | *.csv | Using 22-port configuration of the E5092A. |
Note: All of the csv files are created by the MWA front-end application with the revision 1.11 ("mwa_0111.xls"). The MWA with the revision 1.11 or above is required for customization of the files.