Are there equation examples for ENA Equation Editor?
(SUPPORTED MODELS IN BOLD: E5071C E5072A E5070B/71B E5070A/71A E5061A/62A E5061B E5063A E5091A E5092A)
Yes. The equation samples are listed in the below "EquationEditor_Examples.txt" file.
Please refer to the "HowToUse_EquationEditor_Examples.pdf" file as well that explains how to use the example file text with the Equation Editor function on the ENA.
The E5071C online Help Manual is also helpful - go to the "Equation Editor" section in the Help Manual.
ENA firmware revision 9.10 or later is recommended when using these equation samples. Rev. 9.10 improves the history function and adds more parameters, such as "x-axis data", to the Equation Editor.
Attached files
Equation examples for ENA Equation Editor: EquationEditor_Examples.txt
How to use equation examples: HowToUse_EquationEditor_Examples.pdf
Related links
- E5071C online Help Manual
- Firmware download page: ENA Series Service & Support Home Page