Choose a country or area to see content specific to your location
Application Notes
Most users of test and measurement (T&M) equipment are familiar with programming an instrument over GPIB/IEEE-488. However, now that USB instruments from companies like Keysight Technologies, Inc. are beginning to appear with USB interfaces, many users may want to try USB instead of GPIB. This is because of the ease-of-use and performance advantages of USB when compared with GPIB and other I/O interfaces used in T&M. This article will provide information on how to set up a test system that includes USB instruments and how to program the USB instruments using Virtual Instrument Software Architecture (VISA) I/O library software. Information is also presented about the T&M USB protocol specifications, and how these protocol specifications make use of USB endpoints. Two programming examples are available. One example shows how to use VISA to download an arbitrary waveform to the Keysight 33220A. Another example shows how to use Visual Basic to program the Keysight 33220A to execute a frequency sweep. Both of these Programming USB Instruments examples are available from www. keysight.com/find/33220a in the Drivers and Software section of Technical Support.
Unlock Content
Sign up for free
*Indicates required field
Thank you.
Your form has been successfully submitted.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.